Your automation, our passion.

Categories

Categories

Line Fault Detection without Additional Wiring

From the recording of the process variable to the evaluation in the control system, many errors can occur that can lead to unwanted process states. In this blog post you can find out how isolated barriers from Pepperl+Fuchs detect line faults in the signal circuit without additional wiring.

By |2025-11-06T11:30:14+01:00July 19, 2021|Explosion Protection|

Hardware and Software Features of the R2000 Series 2-D Laser Scanner

The 2-D LiDAR sensors of the R2000 series feature a gapless all-around visibility of 360°. In this blog post we’ll take a closer look at the R2000’s hardware and software features and how these can help solve your individual application.

By |2023-03-03T22:47:49+01:00June 28, 2021|Industrial Sensors|

Configuring the 7500 Series Purge and Pressurization System

The 7500 series is a type Z/Ex pzc purge and pressurization system that enables non-rated electrical equipment to be used in hazardous areas. This blog article shows you how to configure the 7500 system components, i.e. control unit, manifold valve, and vent.

By |2023-03-03T22:39:36+01:00June 16, 2021|Explosion Protection|

How to Prevent Dust Explosions Using Pressurization

One of the best ways to prevent dust explosions is to thoroughly clean the work environment of combustible dust to ensure the safety of the plant and workers. However, equipment operating in enclosures in the plant must also be protected. In this blog post, learn where explosive dust atmospheres occur and how they can be avoided through purge and pressurization systems.

By |2023-08-25T12:27:00+02:00May 25, 2021|Explosion Protection|

Into the Future of 3-D Vision Technology with PXL+

With the PXL+ technology developed by Pepperl+Fuchs subsidiary VMT, however, 3-D point cloud images can be enriched with any number of sensor data. Thanks to this valuable additional information, the gap between human and machine vision can be closed...

By |2023-01-20T15:16:15+01:00April 07, 2021|Industrial Sensors|

Simplifying Thin Client Management with VisuNet Control Center

For automation sites that have implemented a Pepperl+Fuchs VisuNet RM Shell thin-client-based architecture for their HMI systems, VisuNet Control Center can be used to make life more manageable inside and outside of the facility.

By |2023-01-20T15:05:54+01:00February 25, 2021|Explosion Protection|
Go to Top