Your automation, our passion.

Categories

Categories

Ultrasonic Sensor FAQ: Detection Range and Accuracy

To choose the right ultrasonic sensor for a particular application, it is necessary to determine which factors affect the detection range and accuracy of ultrasonic sensors and how incorrect measurements can be corrected.

By |2023-06-07T13:08:04+02:00November 12, 2018|Industrial Sensors, Knowledge Base|

Ultrasonic Sensor FAQ: External Influences on Sensor Operation

How do temperature, rain, and other external factors influence the performance of ultrasonic sensors? Read the blog article below to find out how ultrasonic sensors from Pepperl+Fuchs handle extreme conditions.

By |2022-08-24T08:46:27+02:00October 15, 2018|Industrial Sensors, Knowledge Base|

Ultrasonic Sensor FAQ: Differences between Diffuse Mode Sensor, Retroreflective Sensor, and Thru-Beam Sensor

Different operating modes can be achieved with ultrasonic sensors with switching output by appropriate construction and configuration. Learn more in this blog article about how diffuse mode sensors, retroreflective sensors, and ultrasonic thru-beam sensors work.

By |2023-01-20T12:27:48+01:00September 17, 2018|Industrial Sensors, Knowledge Base|

Five Reasons to Use Industrial RFID in Your Meat Processing Plant

If you want to establish internal food traceability in a meat processing plant, you face a number of challenges: Diverse processes, harsh environmental conditions, hygiene requirements and different transport routes demand a flexible and at the same time reliable technology. Industrial RFID offers a solution for this and also, depending on the application, other additional benefits.

By |2023-10-11T11:36:46+02:00May 12, 2016|RFID, Applications|

What Is a Fieldbus Terminator and What Is Its Function?

The fieldbus terminator, also referred to as a terminator, is a component in a fieldbus system. This terminator takes the shape of a series connection featuring a 1 µF capacitor and a 100 Ω resistor. The main task of the fieldbus terminator is to transform the data signal transmitted as a current change into a voltage change that can be detected by all nodes.

By |2023-10-11T11:26:05+02:00May 10, 2016|Explosion Protection|

Ten Application Examples for RFID in Industrial Automation

RFID is one of the most versatile technologies in industrial automation. Whatever industry you may be thinking of—it is highly likely that RFID will be used there. We have compiled ten RFID applications that give you ideas for possible applications and demonstrate the advantages of this identification technology.

By |2022-08-18T11:53:51+02:00March 30, 2016|Applications, RFID|

Frequently Asked Questions (FAQ) on RFID (Part 4): RFID Tags

RFID tags carry information on a certain object or transport container. The size of an RFID tag can vary from the dimensions of a match head to a brick. While some tags are used simply as an attachable ID for an object, others carry a variety of different attributes relating to the object.

By |2022-08-18T11:50:20+02:00February 29, 2016|RFID, Technologies|

Frequently Asked Questions (FAQ) on RIFD (Part 3): Frequencies

To enable noncontact data exchange via an RFID system, radio waves are used for communication. Depending on the application requirements, RFID systems utilize different frequency ranges. As a general principle, most RFID systems use the so-called ISM bands (Industrial, Scientific, and Medical Band) in order to avoid cross-talk of radio systems and ensure reliable data information exchange. Commonly, passive RFID systems use either low frequency (LF), high frequency (HF), or ultra-high frequency (UHF).

By |2022-08-18T11:48:21+02:00February 25, 2016|RFID, Technologies|
Go to Top