By |November 03, 2022|Categories: Applications, Industrial Sensors|

3 Sensing Methods to Verify Part Ejection in Metal Forming

Content of This Article

3 Sensing Methods to Verify Part Ejection in Metal Forming

When punching or notching metal strips, unwanted material must be cleared before the next press downstroke. If scrap or formed parts inadvertently remain, the press must be stopped before its motion reaches the critical angle, the “point-of-no-return” at which further movement risks damage to the press and die. A variety of precise and reliable sensors are available to protect the die. Keep reading to learn three sensing methods to verify part ejection in metal forming.

Residual metal slugs from metal forming
Residual metal slugs from metal forming
Stripper plate monitoring in metal forming with Pepperl+Fuchs sensors
Stripper plate monitoring in metal forming with Pepperl+Fuchs sensors

Material remaining in the die can cause major tool damage.

Monitor Stripper Plate

During the press downstroke, spring-loaded stripper plates push down on the fed material, preventing it from being pulled upward as the punch tooling retracts. Detecting the presence of the stripper plate during the downstroke using inductive sensors confirms there is no material remaining in the die. A missing stripper plate means that something is preventing the plate from bottoming out and the controller must stop the press.

In order to avoid such errors and machine downtime it is common to install inductive sensors such as the NMB6-F104M in the lower die to detect strippers. Placing a sensor at each corner ensures the die is fully protected, regardless of where an unwanted metal piece is located (here, one or more of the four corners will not bottom-out).

Part Detection on Ejection Chute

Sometimes verifying that a part has been ejected is enough to make sure the die is clear. Monitoring the passage of a workpiece through a chute or its free fall into a bin with a thru-beam sensor, such as the MD17MV17 is all that is required. The ejected part is detected when it breaks the beam.

Confirm workpiece ejection with Pepperl+Fuchs thru-beam sensors
Confirm_workpiece_ejection_Pepperl+Fuchs

Thru-beam photoelectric sensors confirm the workpiece was ejected.

Confirm workpiece ejection with Pepperl+Fuchs light grid sensors
Confirm workpiece ejection with Pepperl+Fuchs light grid sensor

Light grids and slot grid sensors provide a wider detection area.

Reliable Object Detection with a Wide Detection Area

Slot grids sensors such as the RAL150 are also an ideal choice for confirming part ejection. Compared to a single-line thru-beam, they provide a wider detection area, which is helpful when the position and orientation of the ejected parts cannot be accurately controlled. An entire field for object detection and adjustable sensitivity levels enable reliable detection of both very small and larger objects.

Subscribe to our newsletter and receive regular news and interesting facts from the world of automation.

Subscribe