How to Flexibly Design Your Workflows with the Tab-IND Industrial Tablet Series and Modular Accessories
Content of This Article
- The modular accessory concept of the Tab-IND industrial tablet enables customized solutions for a wide variety of use cases in logistics and production.
- With scanner frames, SmartBack extensions, docking solutions, mounts, and carrying systems, the tablet can be flexibly configured for mobile, stationary, and vehicle-mounted applications.
- Companies can deploy a unified device platform and adapt it to changing requirements and work processes.
- This simplifies integration, increases device availability, and supports efficient digital processes.
Depending on the application, industrial workflows place different demands on mobile devices. In logistics, fast barcode scanning and seamless documentation of material movements are crucial. In production, mobile devices assist employees with mounting, material staging, and quality assurance, and provide direct access to digital work instructions and manufacturing information.
The Tab-IND industrial tablet from Pepperl+Fuchs serves as a central, flexibly expandable platform for these purposes. Available in 8- and 10-inch models and with either the Android or Windows operating system, it can be tailored to mobile, stationary, or vehicle-mounted work processes using the appropriate accessories. Scanner frames, docking solutions, mounts, and carrying systems expand the tablet’s capabilities to suit the specific application. The SmartBack interface on the back allows the Tab-IND to be added with additional functions, such as a battery extension or a VESA adapter. This creates a unified device platform that meets changing requirements, reduces integration effort, and supports digital processes throughout the entire value chain.
In this blog post, we’ll show you which accessories are available for the Tab-IND and how they can be used in various applications.

“Scan and Track” with the Scanner Frame
During order picking, goods receiving, material staging, or manufacturing, barcodes need to be captured quickly, allowing the information to be immediately assigned to the corresponding order. When paired with the Scanner Frame—a frame with scanning functionality designed specifically for the tablet—the Tab-IND becomes a high-performance barcode scanner that helps you capture barcodes directly on the tablet and assign them to the corresponding order via the application in use.
Typical applications include scanning cardboard boxes, plastic containers, or components, as well as digitally confirming picking lists, production and shipping orders.
Possible fields of application:
- Order picking
- Inbound goods
- Material staging
- Manufacturing and assembly
- Tool issuance
- Quality control
- Shipping and freight handling
Rugged Frame for Use in Demanding Environments
In manufacturing and logistics, bumps and drops cannot always be avoided. As a rugged protective frame, the Rugged Frame further increases the 10-inch tablet’s drop resistance to up to 1.8 meters and helps ensure that the Tab-IND remains undamaged after such incidents.

Securely Mounted with the Vesa-75 Smartback Adapter
The Tab-IND can be used both on the go as well as in stationary settings or in vehicles. With the VESA-75 SmartBack adapter, you can easily attach the tablet to suitable mounts, such as on machines, walls, or in vehicles. The integrated power supply and USB port simplify integration into the respective infrastructure. This allows the mobile tablet to become a permanently integrated control and information device when needed.
Benefits of the VESA-75 SmartBack Adapter:
- Secure integration into stationary applications in accordance with the VESA-75 standard
- Mounting on machines and workstations
- Suitable for vehicle applications
- Use of standardized VESA-75 mounting options
- Flexible transition between mobile and fixed installations
From a Mobile Tablet to a Stationary Workstation with the Docking Station
With the docking station, the Tab-IND becomes part of a stationary work environment. This provides additional I/O interfaces and charging capabilities at production workstations, control rooms, or logistics stations. As a result, the tablet can be used flexibly on the go or integrated into a fixed infrastructure without having to switch devices. A suitable docking solution is also available for configurations with a scanner frame.
Shoulder Strap and Hand Strap for Improved Mobility
Whether for material supply, quality inspection, or order picking: The shoulder strap makes the Tab-IND a helpful companion in your daily work routine. The tablet is always within reach, while your hands remain free for other tasks. The hand strap also enables secure one-handed operation and facilitates quick access to digital information.
Typical applications:
- Manufacturing and mounting
- Material supply
- Quality inspection
- Order picking
- Inventory
Long Operating Time with an Additional Battery and Charging Solutions
The SmartBack-based lithium-ion battery pack extends the operating time of the Tab-IND 10 by up to 75%. Single and multi-port charging stations, as well as replacement batteries, ensure that the devices are reliably available even when used over long periods or in shift operations.
Scanner, Camera, and Light Bar for the Tab-IND 15
The Tab-IND 15 can also be expanded with optional accessories to suit stationary work processes. The scanner module enables direct barcode scanning at the terminal, for example, to identify components or material containers. The camera module supports visual documentation, such as during quality inspections. With the light bar, status information is visible even from a distance thanks to colored light signals. This allows data acquisition, documentation, and status display to be consolidated at a single workstation.
More Information
Subscribe to our newsletter and receive regular news and interesting facts from the world of automation.